What is the minimum flow rate required for SP submersible pumps?

While operating the pump, an uninterrupted minimum flow rate is required in order to sufficiently cool the pump and the motor. The required minimum flow rate depends on the motor diameter and the well diameter. Please refer to the datasheet of the respective pump for precise specifications regarding the minimum flow rate.