How many switching cycles per hour are allowed without compromising the service life of the SQ/SQE pump?

The number of switching cycles is unlimited, as the SQ/SQE is equipped with soft start integrated into the motor. For this reason, the pump is able to restart immediately after being switched off.


    Facebook Twitter LinkedIn Technorati