Grundfos throws cold water on summer

June 01, 2017

Make good homes great

With summer fast approaching, Grundfos is working with its key dealers and distributors to advise households across the Middle East how to ensure a constant supply of cold water, even at times of peak demand, using the company’s range of high performance domestic water pumps.

From Mid-June onwards, Grundfos will be running a special ‘Cold Water’ campaign with its distributors, focussing on sophisticated and very reliable pumps that have been developed to maintain pressure and continuity in domestic cold water supplies – especially when demand is at its highest.

Homeowners have been putting up with cold water taps that run hot during the summer for years”, said Grundfos’ Sales Director, Andrea Benvenuti. “So this year we are working with our Distributor network to highlight that solutions are available using pumps specially designed to keep water cool and continuous. We’re using the strap line “Make Good Homes Great” because constant cold water availability can transform homes and lifestyles, as well as creating a more comfortable and healthy environment for the family.”

The campaign will focus on the company’s CM, PM and CMBE models – three popular pumps that have proved to be very reliable in providing continuous supplies of domestic cold water to all taps, at all times.

The pumps offer a range of different performance levels and applications. From the compact and modular CM (centrifugal modular pump), which can be used in a variety of configurations to suit virtually any domestic application; to the PM pressure manager and sophisticated CMBE booster with integrated speed control, all have been designed for ease of installation and use in the domestic environment.

The highly efficient pumps will not only save valuable water by managing the supply more effectively, but will reduce energy usage, helping to pay back the initial installation cost.  


    Facebook Twitter LinkedIn